This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: 使用External Pattern Mode,如何解决并行口第N次输入的数据将在N+1次时输出造成的第1次输出图像不能指定的问题?

Part Number: DLPC3478


在使用External Pattern Mode时,并行口第N次输入的数据将在N+1次时输出。第1次输出的图像为默认图像(测试发现),为保证第0次输出的图像也是由外部并行口输入,我本打算在初始化时,直接先通过并行口输入一张图像,用以保证后续每次图片都正常,但是测试时发现,只要两次图像操作的时间间隔超过一定时间,后面操作输出的第1次图像又会变成默认图像。请问,在External Pattern Mode时,可以设置默认图像(外部输入的某一图像)吗或者有其它的解决办法吗?

我们的应用场景是:每次触发,都是连续发送12张不同的图片(是固定的12张图),采用的是External Pattern Mode下的8 bit模式,也就是每次传输3张图,本来只需要传输4次即可完成12张图,但是因为每次触发之前,得发送一张图保证出来的不是默认的图片,导致必须发送5次才能完成12张图,造成效率的下降。