This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我们使用的是 dlp4710 + dlpc3439 系统,
当上位机将 PROJ_ON 引脚置高之后,能投出DLP原始图片,如下图:
但是此时读到的HOST_IRQ电平持续为高电平,也即DLP系统没有初始化完成。通过IIC也不能控制DLPC3439。
请问 1,能投出上图是否说明dlp系统已经初始化完成?
2,如果没有初始化完成,可能的原因是什么?
3,在通过IIC控制dlpc之前,需要的操作是:①上位机将PROJ_ON信号置高,②等待HOST_IRQ引脚变低,③给dlpc发送控制命令 。这个顺 序有什么问题吗,上位机还需要执行其他的操作吗?
非常感谢您