This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3433: DLPC3433+DLPA2000+DLP3010

Part Number: DLPC3433
Other Parts Discussed in Thread: DLP3010, DLPA2000,

我们是做ar眼镜产品的,项目采用一根type c线——》DisplayPort转双mipi——》DLP系统(DLPC3433+DLPA2000+DLP3010)的方式,这种方式供电也来自type c线。我看到DMD对下电的要求比较高,分了normal park和fast park。那像我这种的产品形态,如果突然拔掉type c线,会不会导致DMD损伤?或者有什么方法能够规避掉此问题?

另外关于fastpark,是不是就是应对这种突然掉电的情况?如果要实现fastpark,硬件上面需要如何设计?软件上面是否需要配置相关的寄存器?