Other Parts Discussed in Thread: DLP3010, DLPC3433
我们从官网下载了DLPDLCR3010-G2-MSP430-SW,使用ccs编译烧录之后(未修改任何代码),HDMI就无法使用了。
1)经过示波器测量,hdmi的hpd是有拉高的。
2)it6801寄存器0A的值始终为0x11(HDMI接入情况下)
3)已确认HDMI线是OK的
4)PC能识别到第二屏幕,能获取edid信息
麻烦帮忙分析下是什么原因造成HDMI无法使用的。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们从官网下载了DLPDLCR3010-G2-MSP430-SW,使用ccs编译烧录之后(未修改任何代码),HDMI就无法使用了。
1)经过示波器测量,hdmi的hpd是有拉高的。
2)it6801寄存器0A的值始终为0x11(HDMI接入情况下)
3)已确认HDMI线是OK的
4)PC能识别到第二屏幕,能获取edid信息
麻烦帮忙分析下是什么原因造成HDMI无法使用的。谢谢!
请问用的是DLP3010的EVM板还是你们自己做的PCBA?PC输出的分辨率是什么?最好用720P来测试。还有你的430 source code是哪个版本?我们在DLP3010EVM上测试过HDMI显示是正常的。
我用的板子是DLPDLCR3010-G2 RevB,就是官方的板子。
DLPC3433烧录的固件版本:7.3.3
MSP430软件的版本全称:DPP343xEVM_IT6801_V1.1_01082018_2xI2C_RevC
主要是因为没烧写MSP430的软件之前,开发板是能够进行HDMI的切换并输出图像,从HDMI芯片寄存器0A的值来看,它是没有收到视频信号的。
要是方便的话,把你编译的固件发我烧写试试?