This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

先进光控制系列DLP和显示投影系列DLP在技术参数上有什么不同。



Hi

你好!

如题,谢谢

Sunny

  • 具体DMD具体分析。速度,精度,分辨率,光功率和工作温度和工作波长范围。

    https://www.ti.com/dlp-chip/products.html

    可以对比选择。

    Start evaluating our DLP 3D scan and machine vision products portfolio by leveraging the following resources. 

     Evaluation module
     Typical applications
     Illumination wavelength (nm)
     Display resolution (Max)
     Array diagonal (in)
     Controller evaluation module
     Reference design
     Evaluation module
     Typical applications
     Illumination wavelength (nm)
     Display resolution (Max)
     Array diagonal (in)
     Controller evaluation module
     Reference design
    DLP3010EVM-LC 3D scanning, dental
    scanning, AOI, facial recognition
    420 - 700 0.9 0.3 N/A TIDA-080003
    DLP4710EVM-LC 3D scanning, dental
    scanning, medical imaging, AOI
    420 - 700 2.1 0.47 N/A TIDA-080005
    DLPLCR4500EVM 3D scanning, dental
    scanning, medical imaging, AOI, SPI
    420 - 700 1.0 0.45 N/A

    DLP4500-C350REF

    TIDA-00254

    TIDEP0076

    TIDA-00293

    DLPLCR65EVM 3D scanning, medical
    imaging, AOI, SPI
    420 - 700 2.1 0.65
    DLPLCR65NXEVM 3D scanning, medical
    imaging, AOI, SPI
    420 - 700 2.1 0.65
    DLPLCR67EVM 3D scanning, medical
    imaging, AOI, SPI
    420 - 700 4.3 0.67
    DLPLCR70EVM 3D printing, 3D
    scanning, medical imaging, AOI, SPI
    400 - 700 0.8 0.7
    DLPLCR70UVEVM 3D printing, direct
    imaging, 3D scanning, medical imaging, AOI, SPI
    363 - 420 0.8 0.7
    DLPLCR90EVM 3D printing, direct
    imaging, 3D scanning, medical imaging, AOI, SPI
    400 - 700 4.1 0.9
    DLPLCR95EVM 3D printing, direct
    imaging, 3D scanning, medical imaging, AOI, SPI
    400 - 700 2.1 0.95
    DLPLCR95UVEVM 3D printing, direct
    imaging, 3D scanning, medical imaging, AOI, SPI
    363 - 420 2.1 0.95