Other Parts Discussed in Thread: DLPC3478, DLPA2005
通过i2c配置dlp曝光在27张条纹序列。当dlp的曝光时间超过20000曝光值时,配置返回正确但是dlp没有投光。
ps:应该不是暗时间配置的问题,配置之前会通过命令读取按时间。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
仔细核对软件配置
These are the release notes for the following firmware image file:
Configuration Settings
*Sequence 21 is a special sequence that displays 7-bit patterns. The least significant bit of the 8-bit pattern data will be ignored.
Notes:
*Sequence 6 is a special sequence with zero pre-exposure and post-exposure dark times. (Note: While running this sequence, a dark time equivalent to the exposure time of one pattern will be added at the start of every pattern set.)
Notes:
Notes: