问题如题。输出到LED的电流如下图,导通190ms后关断6ms,而总导通时间只有几秒后DLPA输出就关断了,其上外壳的裸露盘很烫。
我该怎么处理这种情况呢?
DLPA3000是否能够处理这种大电流的输出呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题如题。输出到LED的电流如下图,导通190ms后关断6ms,而总导通时间只有几秒后DLPA输出就关断了,其上外壳的裸露盘很烫。
我该怎么处理这种情况呢?
DLPA3000是否能够处理这种大电流的输出呢?
在驱动大的LED电流时,DLPA3000表面必须要加散热器和风扇,这样才能保证不过热保护。
但是我在不加散热器和风扇直接裸露在空气中的情况下,分别使用DLPA3000C和DLPA3000D的2个板子进行相同的LED输出(使用示波器的电流钳以确定输出电流波形一致),结果DLPA3000C的板子可以坚持很久之后才会热关断,而DLPA3000D只有几秒到几十秒。我现在不确定是型号的原因还是板子的原因,毕竟板子进行了layout的部分调整。您有什么解决思路吗?
而且现在可以看到仅仅几秒6A输出就关断,DLPA3000甚至都来不及传导热量出来。
DLPA3000C芯片在2015年左右已经升级到了D版本,所以建议你使用DLPA3000D。PCB layout的相关要求请参考芯片的规格书。如果你的LED电流为6A,最好是先把散热器和风扇加上再上电。
好的,谢谢!
如果出现过热保护,即达到121.4°和132.5°是否会使得芯片的性能损伤呢?
另外,为何TS_SHUT描述里面会有与V5P0相关的事件呢?
理论上来讲,超过一定温度芯片会自动触发过温保护机制,避免损坏芯片。TS_SHUT会同时监控过温和内部5.0V的状态。