你好,我想知道该型号关于370-420nm波长的反射率以及紫外波段不同区间能承受的最大光功率值是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

可以根据我们datasheet上提供的光功率密度和active array的面积相乘换算一下
第一点,这部分datasheet看到过,就是从这里,加上官网推荐的第三方光机发现了一个问题,第三方有个关机,采用660TE芯片,然后光源波长385nm,最后经过镜头后能达到3W光功率,那这样的换算下来,DMD处<395nm的光功率密度应该远远超过2mw/cm2,所以我就想知道这个应用是定制的660TE还是说他们在缩短寿命的情况下应用的呢?
http://www.wintechdigital.com/index.php?route=product/product&product_id=58
第二点,就是DMD子镜处关于370-420波段的反射率数据有吗?还是说所有波长在子镜上反射率都基本一致?
第三点,datasheet只写了窗口片的420之后的透过率因为该芯片主要应用于显示与透镜,那窗口片镀膜应该是专用可见光膜层,窗口片我是否可以采用下面曲线的反射率作为计算应用?


1. 我们没有专门定制的DMD,在超出我们SPEC值情况下使用DMD都是会影响的使用寿命。
2. 你提供的图片就很好的说明了不同的wavelength情况下反射效率不同,DLP660TE是用于可见光下显示投影的DMD,datasheet上有涂层说明,可以参考这个曲线。

而且DMD的光学效率还有很多其他参数影响,可以参考这篇文章