This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3470: DLPC3470 Write Trigger Out Configuration (92h) 不马上生效

Part Number: DLPC3470


发现一个问题,使用IIC 配置DLPC3470 IO输出,使用了如下步骤:

1、 配置 Write Pattern Configuration (96h),配置投影时间等

2、配置 Write Trigger Out Configuration (92h),使能 Trigger Out 1, Delay时间修改为  Pre-illumination Dark Time

3、配置 Write Operating Mode Select (05h) ,选择外部pattern模式,使以上配置生效

4、然后马上通过RGB24并口传输图像数据到DLPC3470,发现Trigger Out 1并不会生效,IO不会有高电平输出

如果步骤3、4 之间增加一点点延时,sleep(10),Trigger Out 1才可以生效。

该问题在我们以前的板子上不存在,最近生产的板子才出现,所以想查出究竟是哪里的问题? 配置 Write Operating Mode Select 后,一般需要delay多长时间?