Other Parts Discussed in Thread: DLPA2005
我这边使用DLPC150芯片,上电后HOST_IRQ引脚一直不拉低。测试供电是正常的,晶振也起振了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HOST_IRQ一直为高说明系统初始化异常,请检测是否所有的硬件连接都是没问题的,包括LED和DMD。
150芯片还需要连接LED吗,是指PMIC_LED_SEL_1 引脚吗。150芯片有没有办法查询状态之类的,比如它初始化卡在哪里,FLASH、DMD还是其他位置。
建议您检测一下DMD是否连接正常,并且测一下DMD的供电电压及上电时序。
我这边参考的TI的官方设计,即DLPC150+DLPA2005的方案,目前发现DLP2005的1.1V、1.8V、2.5V等输出都正常,但是VBIAS、VOFS、VRST三个电压在反复复位,RESETZ引脚也在复位,大概250ms左右会拉低10ms。下图是RESETZ和VRST的波形图


1.针对这个不断复位问题,我觉得您的DMD可能出现损坏,建议您更换一个新的DMD进行交叉实验验证。
2.请仔细对比您的原理图与参考设计,确认你的DMD与controller之间的option是否一致,否则会出现固件与硬件不一致的问题,导致没有有效数据传输到DMD而无法启动。