This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: Internal patterns 投影时DMD工作状态

Part Number: DLPC3478

您好!

我想了解下DMD3010或4710在Internal patterns 投影时DMD的工作状态,

假设使用Free Running Mode模式,那我发了run once指令后,

DLPC3478是否就开始加载图片数据到闪存,然后DMD开始进行动作?

某一个Pattern在Illuminator打开直至Illuminator关闭的这段时间,此时DMD Pixel是不断动作还是保持一个角度的状态?

投影1bit 或8bit Internal pattern,有区别吗?

我是否可以理解为,在Illuminator打开的时候,DMD上的各个Pixel角度已经准备好,

相机拍照的曝光时间,只需要在Illuminator打开的某个时间段就能拍到下载的Internal pattern。