我们想验证自己的光路结构,但是不清楚如何单独去控制镜片的状态,sdk里面有预留控制镜片翻转的接口出来吗?还是上位机通过指令就能控制呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
是通过MCU和DLPC之间的RGB总线来传输图像并控制微镜的翻转的。DLPC150和DMD之间的通信协议并不开放,目的在于降低客户开发难度以及保护DMD。DLPC150会自动实现将RGB输入的信号转换为DMD能够识别的信号并发送给DMD。可以通过控制输入的RGB信号来控制相应的微镜。
参考设计:
http://www.ti.com.cn/tool/cn/TIDA-00554#technicaldocuments
EVM:
http://www.ti.com.cn/tool/cn/DLPNIRNANOEVM
谢谢
RGB不需要用户控制,只需要将想要投影的视频或图像以RGB888的格式输入给controller就可以,cotroller会自动根据你输入的信号控制DMD翻转和RGB三色灯点亮。