我们都知道DMD每个像素点只有0和1状态,那么单个像素点是如何实现8位灰度图显示?谢谢
sunny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Fortune, 根据文档说描述,8bit灰度图的显示时间应该是1bit的256倍,那为什么DLPC410手册上却说1bit是32KHz,8bit是4KHz,也就只有8倍。请问是如何做到的?
1bit位深只能显示黑或白两级灰度,8bit位深可以显示256级的灰度,与显示时间没有关系。1bit是32khz,8bit自然就是4khz。
Hi Fortune, 这个回答恕我不能理解。根据你之前提供的链接,显示一个8bit的pattern需要256个1bit的时间,这是和时间相关的,如下图所示。如果1bit的刷新率是32KHz,那么8bit的刷新率就是32K/256也就是125Hz。还请详细解释一下,其中的工作原理。

8bit pattern的照明时间是1bit pattern的8倍,不是256倍,您说的这个图是bit plane, 和时间无关。