LED开启后,1.5uH电感啸叫,电路部分参考demo设计,没有更改。输入电压Vin=19V,LED电流设为10A。
更改电感值(目前调试只增大了电感),减小/增大容值,均没有明显改善,请帮忙分析一下,谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LED开启后,1.5uH电感啸叫,电路部分参考demo设计,没有更改。输入电压Vin=19V,LED电流设为10A。
更改电感值(目前调试只增大了电感),减小/增大容值,均没有明显改善,请帮忙分析一下,谢谢!

感谢回答!
10A电流可以正常输出。
调整为1.4uH后还是有啸叫,人耳听到的是这个电感附近,已排除1.8V和3.3V的3.3uH电感。
LED使用恒流源供电,驱动板不会啸叫。请问是否还有其他排查思路,开关频率是否可以调整
开关频率无法调整
是否为layout导致的寄生电容电感太大,电容ESR较高?
如果减小负载,降低电流输出是否有改善?
可以先测量一下开关波形,是PWM包络落在了音频段内还是有其他较大的纹波?