This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3478: 内部Pattern模式如何指定投影的高度尺寸

Part Number: DLPC3478
Other Parts Discussed in Thread: DLP3010,

       DLPC3478+DLP3010

       器件工作在  Internal Pattern Streaming Mode 模式

      现在想修改投影输出的尺寸(只改变高度方向),想改为1280*320(预防多余投影在设备内部有可能的多次反射)

     看了Programmer Guide,有三个尺寸可以指定

1)Write Input Image Size (2Eh)

2)Image Crop

3)display Size

请教如下问题:

1)Write Input Image Size (2Eh)--这是不是仅仅针对External Mode,而对internal Mode,不起作用?

2)Image Crop配置--是不是对Internal Mode也不起作用?

3)display size-

    通过修改display的参数,发现test Pattern Mode下,图像会有变化,但是切换到Internal Mode下,

还是不起作用。

Internal Mode的投影尺寸能进行修改吗,还是限定为1280*720 Full Size的输出?

谢谢