This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果完全断开,VOFS和VBIAS完全没有电压。VRST电压0.2V.连接DLP3010,电压用示波器查看,VBIAS可以到18V和VOFX可以到10V,但是VRST只能到-5V,无法达到-10V。麻烦再分析一下,谢谢!!
如果完全断开,VOFS和VBIAS完全没有电压。VRST电压0.2V.连接DLP3010,电压用示波器查看,VBIAS可以到18V和VOFX可以到10V,但是VRST只能到-5V,无法达到-10V,同时V6V这个管脚没有电压输出。麻烦再分析一下,谢谢!!