This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010: 关于dlp3010 固件的一些疑问

Part Number: DLP3010
Other Parts Discussed in Thread: DLPA300, DLPC3478, DLPA3000, DLPA2005,

在使用官网固件的dlp3010的evm测试时,可以下载超过2个pattern set的8bit 灰阶竖条纹,每个set 6张条纹,

我这边实测下载了6个pattern set ,并工作正常。

固件版本如下图:

但是我们实际开发的是采用DLP3010+DLPC3478+DLPA300的硬件,固件采用的是官网Firmware Selector生成的固件,如下图所示:

使用这个固件,最大只能下载2个pattern set的8bit 灰阶竖条纹,再多就提示超范围了,

请问这两个固件版本有何区别,能否提供下基于DLPA3000的能下较多pattern set的固件,用于3d扫描,谢谢。