This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC300: DLPC300使用Multiple Bit Depth and Multiple Color Pattern Sequences功能的问题

Part Number: DLPC300
Other Parts Discussed in Thread: TMS320DM365, DLP3010LC

工程师,您好,我有一个问题想请教你们, 我手上有DLPC300和DLP3000的芯片,和做好的板子,我现在板子上有FPGA,MSP430,DLPC300和一片st公司的ARM(M4),但是板子上没有TMS320DM365。我想实现

Multiple Bit Depth and Multiple Color Pattern Sequences的功能。我看了TI官方提供的操作方法是使用 DLP LightCrafter GUI 通过usb下载到TMS320DM365,再由TMS320DM365解析传到DLPC300,因为我的板子上没有TMS320DM365这颗芯片,我想是否可以只用FPGA  ,msp430 再加上我的ARM(M4内核)完成Multiple Bit Depth and Multiple Color Pattern Sequences功能。

第二点:或者是否能提供FPGA和TMS320DM365的源代码,我看是否能自己修改,因为我只找到MSP430这颗芯片源代码,因为我使用不同的FPGA就不能使用贵公司提供的.rbf文件,需要从新开发。