This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC900: DLPC900 的FlashDeviceParameters.txt如何配置?

Part Number: DLPC900

您好:
我们做了DLPC900的新板子,采用了Infineon的 S29GL512S,64MB,其逻辑门电路也按照规格书64M的配置修改了。
现在不知道JTAG的配置文件FlashDeviceParameters.txt如何配置才能正确下载bootloader
原EVM采用S29GL512S ,原文件中配置参数 Total number of sectors 写的是128,
但是查看S29GL512S 的规格书,这芯片的Total number of sectors是2048,为什么不一样?

我们对S29GL512S写的配置如下:
"Cypress", 0x0001, 0x0000000000000001, "S29GL512S", 0x227E, 0x000000000000227E, 64, 0, 0x800000, 128, 0x0, 0x10000, 0x20000, 0x30000, 0x40000, 0x50000, 0x60000, 0x70000, 0x80000, ......
但是这个配置不能正常启动。
请问,对于我们采用的S29GL512S,64MB,正确的FlashDeviceParameters.txt应该怎么写? 谢谢!