This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: I2C问题

Part Number: DLP4710EVM-LC


光机上电,CY_IIC0_SCL 有波形,CY_IIC0_SDA也有波形。

去掉R654,R655,CY_IIC0_SDA没有信号,IIC0_SDA有信号。

问题1:上电后,这个I2C_SDA貌似是3479发出来的,它发的是什么东西呢?

问题2:电平转换U44,B端上拉10K,A端为啥上拉的是2.2K ? I2C信号上拉2.2K、1.5K见的较多,10K上拉很少见啊。

我们有块板,被另一个ARM板通过USB口触发,碰到了运行一段时间后I2C信号CY_IIC0_SDA量不到的情况,不是经常出现,很难得出现一次。出现后,就触发不了投光了。与上拉电阻有关系吗?

 

  • 1,EVM 板上有一个MPS430的MCU,上电时可能会配置IT6801的寄存器,所以你会测到I2C上的波形。

    2,EVM板上I2C实际的上拉电阻是2.2K;10K的那些是NC的。这个电阻和光机不投光应该没有关系。