This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: 使用DLP4500 GUI / 350 无法连接光机设备

Part Number: DLP4500


在linux下开发过程中, DLP4500 GUI 无法连接光机,出现错误提示如下:

     open device_handle error: Is a directory
     opening path [/dev/hidraw5]
     error number: 21

或者

    open device_handle error: Is a directory
    opening path [/dev/hidraw6]     
    error number: 21

USB 线拔掉再插也无法解决问题,只要出现这个问题,自己编写的光机程序或则官方的DLP4500 GUI 都无法连接成功

只有重启机子有时会恢复正常,但这不是办法,如果产品一直存在这种潜在的问题,客户体验是非常致命的。

请教这个问题的解决方法,该如何处理?