This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS99000S-Q1: DMD_VRESET,DMD_OFFSET,VDD&VDDI带载时高低电平电压幅值超限

Part Number: TPS99000S-Q1
Other Parts Discussed in Thread: DLP5530S-Q1

    我们在测试TPS990S-Q1输出给DMD DLP5530S-Q1的电压VOFFSE和VBIAS的时候遇到一些问题,具体如下:
    在DLP5530S-Q1的datasheet中,VOFFSET推荐的工作电压范围是8.25V~8.75V,typ 8.5V;VRESET推荐的工作电压范围是-9.5V~-10.5V typ -10V,VDD&VDDI推荐的工作电压范围是1.7V~1.95V typ 1.8V。
    然而我们在实际测试中测量VOFFSET高电平的波动范围是7.945V~8.661V,高电平的下限值低于推荐值8.25V。测量VRESET的低电平的波动范围是-9.54V~-10.06V,超出了-9.5V的推荐电压范围。测量VDD&VDDI的高电平波动范围是1.444V~2.336V,超出了1.75V~1.95V的推荐电压范围。
    电源滤波电容,电阻的选型都是根据参考设计选型,并且我们在TI DLPC230的开发板测出的波形同样不能满足DMD推荐的工作电压范围。
    想请教下出现这种波动的原因是什么?是否和DMD的工作原理有关?如果超出推荐的工作电压范围会造成什么问题,以及建议如何优化?
    具体测试波形如下图:
    VOFFSET带载波形:
VRESET带载波形:
VDD&VDDI带载波形