This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC230-Q1: 在我们的PGU中,R、G、B灯的动态范围在一帧内不一致

Part Number: DLPC230-Q1


朋友们,大家好!

我们使用基于 DPLC230 + TPS99000 芯片的系统,我们测量了LED_SEL (3:0) 信号在一个帧时间内处于活动状态的时间长度。具体来说,驱动R、G和B的信号LED_SEL动态范围等于信号LED_SEL在一个帧时间内分别分配给R、G和B的总驱动时间和最短驱动持续时间之比。因此,我们得到以下测量结果:

数据表明,红光的动态范围为256.52,绿光的动态范围为263.78,但蓝光的动态范围为128.07。一般来说,R、G、B的动态范围应该不一样吧?造成这种现象的原因是什么?谢谢!