The current phenomenon as the following goes:
I powered up the module, press the ON/OFF button, wait for 3 seconds and the lens will start to display,
Then the startup interface of the application will appear,
But the display will automatically turn off after about 2 seconds.
And here is phenomenon and order of LED lights
POWER UP:
D43 ON INTZ(D57)ON
PRESS THE ON/OFF BUTTEN:
D43 OFF INTZ(D57)OFF
D56 BRINK ONCE
D33 ON & Len start to display
Len turn off after about 2 sec
D33 OFF D56 BRINK ONCE
D43 ON INTZ(D57) ON
I have tried for many times but it still can not start working normally.
I also have tried to reprogram the module by the frimware on homepage, but it didn't work.