Other Parts Discussed in Thread: DLPA2005, DLPC3478, ,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我手头一个前年买的EVM,里面配的DLP3010是旧版本的。那么现在我将EVM上的DLP3010FQK更换为新的DLP3010AFQK之后,使用新固件应该就可以吧?
我看之前的EVM版本是
FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v8p0p0.img,现在是FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v8p0p1.img,即下图,对吗?

非常感谢您的回答。
然而我司于前年购买的DLP3010-LC EVM拆下光机部分的DMD之后发现其DMD的实际型号是DLP3010LCFQK。我成功下载了固件FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v8p0p1.img,可以连接DLP3010LCFQK或者DLP3010FQK,但是当我安装了DLP3010AFQK之后反而不行了,不能输出splash screen,也不能识别I2C:

FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v8p0p1.img难道不是最新的固件吗?理论上不管能不能识别到旧版本的DMD但肯定应该能识别到带A的新DMD了呀?
还是3010的EVM除了固件还有硬件上的改变?
另外,DLP3010LCFQK,DLP3010FQK与DLP3010AFQK有什么区别呢?贵司是有三种型号吗?
我再次排查了固件的选择,发现下载的适用于DLPC3478控制器+DLPA2005的v8版本的固件都是绑定于DLP3010LC的,如下图,那么可能v8固件就是无法驱动DLP3010AFQK.
根据此链接,需要v7版本才可以驱动DLP3010AFQK,不知道我是否理解正确?
若是正确,那么下图的selector已经无法获得v7版本,怎么才能获得适用于DLPC3478控制器+DLPA2005的可以驱动DLP3010AFQK的固件呢?

谢谢回复,应该是我对论坛的操作出现了失误。
只是抱歉产生了困惑。
目前的EVM都是最新的固件,适配DLP3010AFQK?:从正规渠道购买的EVM板目前都更新了
但是另一个问题里面:
购买的DLP3010EVM-LC拆开后发现是DLP3010LCFQK,是否它能支持DLP3010AFQK呢?
您的回答是:新出的固件都不支持