This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: 是否可以提供7.0版本固件?

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLPA2005, DLPC3478, DLP3010, DLP3010LC, DLPC3438, DLPDLCR3010EVM-G2, DLPC3433, DLPA3000

从下面的链接得知:

使用DLP3010AFQK需要使用7.0版本或以上的固件,7.0或以上的固件同样可以支持DLP3010FQK。

DLP3010AFQK和DLP3010FQK的区别 - DLP®︎ 产品论坛 - DLP 产品 - E2ETm 设计支持 (ti.com)

那么是否可以提供DLP3010EVM-LC的7.0版本固件呢?

其组成为DLPC3478+DLPA2005+DLP3010AFQK

我从fimware selector里面只能找到8.0版本以上的,可惜的是并不能识别DLP3010AFQK