This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: 修改官网单灯固件的输出占空比(duty cycle)

Part Number: DLPC3479


你好,请教一个问题,我在官网上下载了一个dlpc3479+3005+4710lc的单灯(红灯)固件,下载到自己画的板子里面可以跑起来,通过示波器测量发现红灯的除数占空比只占了23%,我想调整rgb中红灯的输出占比(起码调整到90%以上),绿灯蓝灯的占比拉低或者直接不需要(我只需要单色),满足我的使用需求,请问怎么才能调整这个占比?

另外,我这dlp composer这个软件中,看到有类似duty cycle的修改,我是否可以通过修改这里达到我想要的效果,我尝试修改发现软件有限制不能给我这么修改。而且不明白他的含义,他有好几个index(cool,warm等),这些代表什么含义,不同色温下rgb的占比?这些色温软件又是通过什么方式选择的呢?