TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3470: dlpc3470 Splash Pattern 模式为什么会设置最大 Pattern 周期,这个最大周期能否更改?

Part Number: DLPC3470
Other Parts Discussed in Thread: DLPC3430, DLP3010LC, DLPC3478, DLPA2005, DLP2010LC

dlpc3470 Splash Pattern 模式为什么会设置最大 Pattern 周期,这个最大周期能否更改?

  • 你说的是light control模式,为了针对3D 打印和3D扫描的一种模式,这个模式下,图片是有曝光周期的,然后有触发信号触发工业相机等外围设备。如果只是想显示一个splash图片可以直接使用display模式或者DLPC3430芯片。具体参考datasheet和programmer guide.

  • 这个应用上是需要触发工业相机,但是针对高分辨率的卷帘相机,帧率比较低,限制最大曝光周期相当于限制了最小帧率,这样搞导致无法正确的触发相机,从而导致图像出现错误。虽然Spalsh 模式确实只是起到显示作用,但是是希望这种显示能够通过相机进行观察。不清楚设置最大触发周期的意义是什么,这个能否进行更改?

  • 参考固件说明:

    https://software-dl.ti.com/dlp/pico-fw-selector/release_notes/FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v8p0p1.html

    DLPC3478 Firmware v8.0.1 Release Notes

    March 14, 2022

    Table of Contents




    Overview



    These are the release notes for the following firmware image file:

    • Firmware Version: 8.0.1
      • Embedded Software Version: 8.1.0
      • Generated from DLP Composer Version: 13.13
    • DMD: DLP3010LC
    • Controller: DLPC3478
    • PMIC: DLPA2005

    Configuration Settings

    • I2C Address: 0x36
    • DMD Pin Mapping: 1
    • Rlim value: 39mΩ
    • Light Control Sequence Database Version: 0.5.71

    Supported Features



      • Light Control
        • Internal Pattern Streaming Mode: - Trigger-In/Free-running modes (Mono 1 Bit/8 Bit, RGB 1 Bit/8 Bit, Vertical + Horizontal Pattern Generation, Pattern Invert)
        • External Pattern Streaming Mode (Mono 1 Bit/8Bit, RGB 1 Bit/8Bit)
        • Zero dark time external pattern display for illumination time less than 400 uSec
        • Splash Patterns (Mono 1 Bit/ 8 Bit)

      • Display
        • External video input
        • IntelliBrightTm video processing algorithms
        • Splash Screens
        • Source frame rates supported - 0 to 123 HZ
        • Four 2D looks (cool, medium, warm, and other) and one 3D look

      • Supported pattern timings in Sequence Database v0.5.71:

        • Internal Pattern Mode Timings:

          Pattern Type
          Sequence Index
          Exposure Time Range (us)
          Sequence Min Pre-Exposure Dark Time (us)
          Sequence Min Post-Exposure Dark Time (us)
          1-bit Monochrome
          18
          200 - 399
          171
          31
          17
          400 - 799
          171
          31
          16
          800 - 799
          171
          31
          15
          1800 - 3799
          171
          31
          14
          3800 - 7600
          171
          31
          1-bit RGB
          25
          600 - 1799
          171
          31
          24
          1800 - 3799
          171
          31
          23
          3800 - 7600
          171
          31
          8-bit Monochrome
          20
          3464 - 6928
          171
          31
          21*
          1677 - 3463
          171
          31
          8-bit RGB
          22
          10912 - 21824
          171
          31

          *Sequence 21 is a special sequence that displays 7-bit patterns. The least significant bit of the 8-bit pattern data will be ignored.

          Notes:

          • For internal patterns, there will be an additional variable delay of ~3000 us at the beginning of every pattern set.
          • Exposure times shorter than the above values are not possible. Longer exposure times will operate with decreased timing accuracy and behavior is not guaranteed.
          • Shorter dark times are not possible. Longer dark times can be used. The maximum possible dark times for a desired exposure time are:
            • Tmax pre-exposure dark time  = ( 27306us + tsequence min pre-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
            • Tmax post-exposure dark time = ( 27306us + tsequence min post-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
        • External Pattern Streaming Timings:

          Pattern Type
          Sequence Index
          Exposure Time Range (us)
          Sequence Min Pre-Exposure Dark Time (us)
          Sequence Min Post-Exposure Dark Time (us)
          1-bit Monochrome
          6
          200 - 400
          0*
          0*
          5
          200 - 399
          171
          31
          4
          400 - 799
          171
          31
          3
          800 - 1799
          171
          31
          2
          1800 - 3799
          171
          31
          1
          3800 - 7600
          171
          31
          1-bit RGB
          11
          451 - 799
          171
          31
          10
          800 - 1799
          171
          31
          9
          1800 - 3799
          171
          31
          8
          3800 - 7600
          171
          31
          8-bit Monochrome
          7
          2555 - 5110
          171
          31
          8-bit RGB
          0
          10912 - 21824
          171
          31

          *Sequence 6 is a special sequence with zero pre-exposure and post-exposure dark times. (Note: While running this sequence, a dark time equivalent to the exposure time of one pattern will be added at the start of every pattern set.)

          Notes:

          • Exposure times shorter than the above values are not possible. Longer exposure times will operate with decreased timing accuracy and behavior is not guaranteed.
          • Shorter dark times are not possible. Longer dark times can be used. The maximum possible dark times for a desired exposure time are:
            • Tmax pre-exposure dark time  = ( 6553us + tsequence min pre-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
            • Tmax post-exposure dark time = ( 6553us + tsequence min post-exposure dark time ) * (Tdesired exposure / tsequence minimum exposure)
        • Splash Pattern Mode Timings:

          Pattern Type
          Sequence Index
          Exposure Time Range (us)
          Sequence Min Pre-Exposure Dark Time (us)
          Sequence Min Post-Exposure Dark Time (us)
          1 -bit Monochrome
          13
          793 - 1744
          171
          31
          8-bit Monochrome
          12
          7737 - 17034
          171
          31

          Notes:

          • The maximum pattern period (pre-exposure + exposure + post-exposure) cannot exceed 2184us for 1-bit splash patterns and 17476us for 8-bit splash patterns.
        • The listed minimum dark times are applicable for the minimum exposure time of each sequence. The dark times scale along with the exposure time as per the following equation:
          • Tmin required pre-exposure dark time  = tsequence min pre-exposure dark time * (Tdesired exposure / tsequence minimum exposure)
          • Tmin required post-exposure dark time = tsequence min post-exposure dark time * (Tdesired exposure / tsequence minimum exposure)

        • I2C command 0x9D (Read Validate Exposure Time) returns the minimum required pre-exposure and post-exposure dark times for a specific pattern type and given exposure time.

    Updates in this release



    • Firmware will support the systems with the Light Control DMDs (DLP2010LC, DLP3010LC) only.
    • Auto-idle mode is not supported.
    • Only DMD pin mapping options 1 and 2 are supported.
    • The corruption observed in internal pattern mode while running 200us zero dark time pattern sets has been fixed.
    • Patterns are only supported in RGB format (not YCbCr) when running in Splash Pattern mode.
    • Thermistor processing enabled by default

    Known Limitations



    • Internal Patterns 8 bit RGB sequence - post dark time does not match specified value.
    • Non uniformity is seen at the display borders while running 1 bit internal patterns with 0 pre,post exposure times.
    • External Streaming - Signals/Patterns Incorrect in case of VSYNC jitter.
    • When switching from internal pattern mode to splash pattern mode make sure that the internal pattern display is stopped.
    • While using the update firmware feature of GUI, make sure that size of splash image are as small as possible and prefer selecting RGB color space if the images are of PNG format.
    • LC splash pattern dispaly is only supported in RGB format.
    • Only RGB888 input source format supported in External Pattern Streaming Mode.
    • Unsupported Features:
      • DSI/BT656 Input
      • CPU Interface
      • LABB with Ambient Light Sensor support
      • Shallow Gradient
      • White Point Correction
      • I2C at 400KHz
      • Flashless configuration
      • Idle mode
      • Power management, clock gating and scaling
      • CAIC is not supported in LC, system will not boot up in LC mode with CAIC enabled

    Technical Support and Product Updates



      • Thermistor Processing Documentation

        • Using System Temperature via I2C commands:
          • Read System Temperature (0xd6)
            • Output: 2 Bytes
              • Byte 1: LSB
              • Byte 2: MSB
          • Note: The temperature of the thermistor is read in degrees Celsius in a magnitude of 10 times the reading of thermistor. Bit 11 (the most significant bit) denotes the sign temperature. A '0' means a positive temperature, while '1' denotes a negative temperature.
            • Example #1: b(11:0) = 000110101010; 426d / 10d = 42.6degC
            • Example #2: b(11:0) = 100110101010; 426d / 10d = -42.6degC
          • Note: This temperature reading will need to be calibrated per the design and specific thermsitor chosen of custom boards. Offset to determine the true temperature of the thermistor reading. Texas Instruments DLP hardware uses Murata's NCP15WF104F03RC.
      • Additional Links



    TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and embedded processors, along with software, tools and the industry‘s largest sales/support staff.

    © Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
    Trademarks | Privacy policy | Terms of use | Terms of sale