Other Parts Discussed in Thread: DLPC3438, DLPA2005, , MSP430F2274, DLPDLCR3010EVM-G2, DLPC3433, DLP2010
您好:
我在设计DLP3010时遇到了一些问题,我参考的是DLPDLCR3010EVM-G2的原理图,在硬件设计方面我做了一些调整。我使用的方案是MainBoard使用的是msp430f2274+it6801,DisplayBoard使用的是DLPA2005+DLPC3438+DLP3010。目前我遇到以下几个问题。
1:在MainBoard部分,我下载的是(DLPC3435-MSP430-v1.0.0-2014-07-29)这个版本的演示代码未做任何修改。在没有连接DisplayBoard的时候测试,当连接PC端的HDMI接口是,PC端并不能识别第二屏幕,但测量HPD引脚大约有3.3V左右的电压,请问这是什么原因造成的?是必须要连接DisplayBoard板之后,PC端才能识别第二屏幕吗?
2:连接DisplayBoard板子后测试,固件使用的是(FWSel_DLPC3433_DLPA2005_pm1_i2c0x36_v7p4p3),已连接DMD芯片,以及连接了LED,发现DLPA2005的VOFS,VBIAS只有4V左右的输出,VRST输出也不正常,LED_1,;LED_2无输出, PROJ_ON 变为高电平后,HOST_IRQ一直为高。假设不连接DMD的情况下,VOFS,VBIAS,VRST的电压正常是多少?请问DLPC3435-MSP430-v1.0.0-2014-07-29这个版本的代码是不是不能直接驱动DLP3010,而是只能驱动DLP2010,如何我想驱动DLP3010需要对代码进行哪些修改?
3:我对硬件做了如下修改(请见附件),是否有不正确的地方?