This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3310: DLPC3437

Part Number: DLP3310
Other Parts Discussed in Thread: DLPC3437

  • DLP3310模组里面为什么用了Master和Slave两个3437片子驱动DMD?作用分别是什么?
  • 如果用此套件做二次开发,是否涉及到fpga的程序开发?
  • 红绿蓝LED的打开和关断是同步什么信号来切换,还是说一直在打开状态中!
  • 谢谢回复,
  • 1.分辨率比较大,要传输1080p的信号,分两个controller进行处理,分别控制一半DMD。

    2.FPGA程序是打包好的,直接下载,没有接口也不需要进行改动

    3.DLPC3437通过SPI控制DLPA芯片控制LED enable信号