我在下列链接中看到DLPD4X00KIT套件适用的DLP芯片组有0.55" XGA,是否意味着DLP 5500可以用D4100套件驱动?
问题是D4100套件的数据速率高于DLP 5500的。如果不能用上述套件,请推荐其它适用于评估DLP 5500的套件(LightCommander已停产)。谢谢关注。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在下列链接中看到DLPD4X00KIT套件适用的DLP芯片组有0.55" XGA,是否意味着DLP 5500可以用D4100套件驱动?
问题是D4100套件的数据速率高于DLP 5500的。如果不能用上述套件,请推荐其它适用于评估DLP 5500的套件(LightCommander已停产)。谢谢关注。
谢谢关注DLP技术。
Discovery 4100的开发套机只支持.7 XGA和.95 1080p,并分别针对可见光和紫外光。.55 XGA需要第三方的设计公司提供定制的模块。我们会尽快更新网站的信息,带来的不便请见谅。
不清楚你们的具体应用是什么?如果.7 XGA可以满足你们的要求,建议用.7 XGA,搭配4100可以提供很高的数据带宽和刷新率。
你好,请问一下,我们使用的也是Discovery 4100的开发套件。我们原有一块0.55 XGA DMD,现在打算更换成0.7XGA的。
请问兼容性上有无问题?除了更换DMD以外,排线和底座模块需要更换吗?谢谢~