Part Number: DLP3010
Other Parts Discussed in Thread: DLPC3433, DLPA2000, , MSP430F2274, DLPDLCR3010EVM-G2
您好:
参考DLPDLCR3010EVM-G2原理图自制了两块PCB板,使用方案为:dlp3010+dlpc3433+dlpa2000,mainboard端使用的是MSP430F2274+IT6801(原理图做了一些改动),如附件所见4162.DLP.pdf,使用的是DLPC3435-MSP430-v1.0.0-2014-07-29这个版本的代码(未作任何修改),经过一些测试,发现如下情况:
1:displayboard端目前测试HOST_IRQ为低,RESET为高,RGB可以常亮,感觉似乎初始化已经成功。
2:当接入hdmi信号时(不论是否接入displayboard),PC端可识别出第二显示器(如下图),可是未能检测出有视频信号输出,msp430的P3.6引脚持续为高电平,当我尝试按键切换成hdmi输入模式时,发现P3.6也未能变成低电平,波形如下图。请问是不是因为原理图哪里修改的不对?

3:无论是否接入HDMI以及displayboard板,MSP430的IIC一直有读写操作,波形如下图,请问这是什么原因?

4:我尝试显示内部测试图像,测试方式是使用msp的UP按键切换显示模式,也未能得到显示画面(如下图),起初我以为是IIC通信有问题,当我使用按键调试RGB电流时,可以得到很好的反馈。请问新下载的固件里自带内部测试图像吗?如果有自带的测试图像,像这样的情况我应该如何去排除故障?