This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710: DLP4710和DLP4710LC

Part Number: DLP4710
Other Parts Discussed in Thread: DLPDLCR4710EVM-G2, , DLPC3439, DLPC3479, ,

您好:

我们想用0.47的DMD开发投影光机,目前从咱们TI的官网买了开发套件DLP4710EVM-LC DLP®4710光控制评估模块,在当时选型的时候,同时也看到了另外的一个套件,DLPDLCR4710EVM-G2全高清 DLP4710 芯片组评估模块,我对比了一下两个套件,发现它们用的方案基本是一样的,除了DLP驱动芯片,一个用的是DLPC3479,一个用的是DLPC3439。在这里我有几个问题想再咨询一下:

1、我看到4710有两个型号,DLP4710和DLP4710LC,那么在两个套件中的DMD是不是一样的呢?

2、如果两个套件用的DMD型号不一样,DLP4710EVM-LC DLP®4710光控制评估块这个套件能用来控制DLP4710投影显示吗?

回复为盼,谢谢!