This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我采购了DLPNIRSCANEVM模块,准备在其上进行开发研究,由于对这个产品及linux系统并不熟悉,在开始开发前我想先了解下两个关键的问题:
I have purchased the DLPNIRSCANEVM module and am preparing to conduct development research on it. As I am not familiar with this product and Linux system, I would like to understand the following two key issues before starting development:
1. SDK资料(ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin)里是否有DLPNIRSCANEVM模块中AM3358上运行的程序源代码?
1. Does the SDK(ti-sdk-am335x-evm-06.00.00.00-Linux-x86-Install.bin) include the firmware program source code for the DLPNIRSCANEVM module
2. 如果我根据DLPNIRSCANEVM模块的参考资料(www.ti.com/.../TIDA-00155)把所有的电路都生产出来,是否能使用sdk里的资料和NIRscan version 2.0完成对新电路板的烧写,从而替换原来的电路板使用起来?
2. If I refer to the DLPNIRSCANEVM module's reference materials( www.ti.com/.../TIDA-00155 )Can all the circuits be produced using the data in SDK and NIRscan version 2.0 to complete the burning and writing of the new circuit board, thus replacing the original circuit board for use?
我现在已经安装了WVware 16.2和Ubuntu虚拟机的安装,如果sdk里面包含了DLPNIRSCANEVM的程序源代码,该如何得到这部分内容并使用开发?
I have now installed WVware 16.2 and Ubuntu virtual machine installation,If the SDK contains the program source code for DLPNIRSCANEVM, how can I obtain this part of the content and use it for development?