Part Number: DLPC3439
Other Parts Discussed in Thread: DLP4710, , DLPA3005, DLPC6540, DLP471TP
您好:
我看到在DLP4710 Gen2的方案中,使用的是DLPC3439+DLPA3005的方式,我也在论坛上看到关于DLPC3439和DLPA3005的组合的一些问题,在这里我想咨询一些如下问题:
1、DLPC3439和DLPA3005必须配合使用吗?如果分开用是否可以?
2、我们的光源电压是30V,DLPA3005的输出达不到这个电压,我想用另外的驱动方式驱动光源,但是DMD的驱动ASIC还是用DLPC3439,这样做是否可以?
3、一个DLPC3439加两片DLPA3005,这样组合能用吗?DLPC3439和DLPA3005之间上电的时候是不是要通信?这个通信程序是在3439中吗?
谢谢!