Part Number: DLPC3478
Other Parts Discussed in Thread: DLP3010LC, DLP3010
DLPC3478控制器不读取SPI0 FLAH,SPI0 FLASH的PCLK没有任何信号,系统加载不起来。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电源已经测试了是正常的。proj_on打开后,SPI0 的CLK引脚没有任何信号。
相关帖子bug原因是因为DMD型号使用错误,你用的DLP3010还是DLP3010LC?
DLP3010LC,之前做过一板,现在新做了一批,只把Parallel Interface的信号线接了出来,用的DLPC与DLPA、光机都是同一种料,新做的板子启动不了。初步定为还是DLPC3478那里的问题,电源1.1V、1.8V、3.3V都测量过没问题,然后24MHz时钟也测试过,INTZ与RESETZ也测试了,都是拉高了,但是DLPC3478就是不启动,SPI0与SPI1均没有信号。
可以排查一下proj_on信号有没有真的送到DLPC3478,找非常靠近DLPC3478的管脚GPIO_08的地方去测量,所有的电压和intz,resetz都是DLPA的输出,所以怀疑是DLPC3478没有真正的启动,要么没有接收到上电信号,要么贴片有问题