This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: 速度与图片大小传输时间

Part Number: DLPC3479

规格书中提到速度:High speed pattern rates up to 1440 Hz (1-bit) and 180 Hz (8-bit)。 支持最大图片是1080P(1920*1080),  

通过并口传输,在RGB888模式下,图片大小为1920*1080*24bit, 如果时钟频率是100MHz,需要多久能传输完毕?和速度1440 Hz (1-bit) and 180 Hz (8-bit)有何关系?多谢