在软件“DLP EVM GUI 3.2.0.6”中设置为“Switch to External Video”,当4710EVM-LC的HDMI接到笔记本电脑的HDMI口时,笔记本电脑设置为“仅第二个屏幕”,此时投影为电脑显示界面的上下重复叠加;笔记本电脑设置为“扩展”或“复制”,投影仅显示4710的预存静态图片。
而将4710EVM-LC的HDMI接到台式机电脑的HDMI口,作为唯一的屏幕时,显示都是正常的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在软件“DLP EVM GUI 3.2.0.6”中设置为“Switch to External Video”,当4710EVM-LC的HDMI接到笔记本电脑的HDMI口时,笔记本电脑设置为“仅第二个屏幕”,此时投影为电脑显示界面的上下重复叠加;笔记本电脑设置为“扩展”或“复制”,投影仅显示4710的预存静态图片。
而将4710EVM-LC的HDMI接到台式机电脑的HDMI口,作为唯一的屏幕时,显示都是正常的。
还是不行。
显示器2设置为1920x1080@60HZ,win10系统识别出显示器2为ITE6801,软件“DLP EVM GUI 3.2.0.6”的“Video information”get的参数:
Input Size: 1280 pixels × 720 lines
Cropping: x=0, y=0, 0 pixels × 0 lines
Display Size: x=0, y=0, 1920 pixels × 1080 lines
Frame Rate: 60.06