This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9500设计问题

Other Parts Discussed in Thread: DLPA200, DLPC410, DLP9500

大家好,

因为从来没做过DLP相关设计,因此在设计时遇到几个问题不确定,请指点

1.DLPA200的数据手册上指出IRQZ管脚(pin43)应该与其控制器连接,控制器就是DLPC410,但在DLPC410的数据手册上,并未提供相应的管脚。请问IRQZ管脚应该怎么连接?
2DLPA200的中Vreset_rail,Voffset_rail,Vbias_rail都是输入管脚,并且与Vreset,Voffset ,Vbias内部隔离,请问这3种管脚应该提供怎么样输入。(按数据手册定义他们应该是由DLPA200生成的电压)?
3.DLP9500的power float 管脚应该最好怎么连接? MODE_A (J1),  MODE_B(G1)应该怎么连接?
4. DLPC410的VLED0,VLED1管脚(还有其他LED灯的连接) ,上面注释都写了连接到一个LED灯,并与22.1欧姆电阻连接,上拉到2.5V。这样上拉的话,VLED0,VLED1必须为LOW才会点亮。可手册上写的是High才点亮,这里是不是有矛盾。还是我自己理解错误?