Part Number: DLP4710
Other Parts Discussed in Thread: DLPA3005
您好:
我们用DLP4710A-G2套件做实验,上电后光机闪一下就没有反应了,供电19V,在打开投影开关时,电流是0.12A左右,测了一下DLPA3005芯片的输出,1.1V,1.8V都有输出,
VBIAS = 18V
VOFS = 10V
VRST = -14V
这几个电压都没有输出。
请问下,这种现象可能是什么哪里的问题导致的?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.