Part Number: DLPC3478
Other Parts Discussed in Thread: DLPA2005,
平台DLPC3478 + DLPA2005 + DMD3010LC
目前为止采用FW8.0.1版本,对应的API为DLPC-API-1.10-Setup
现在FW升级到9.0.1 : FWSel_DLPC3478_DLPA2005_pm1_i2c0x36_v9p0p1
修复了Internal Pattern Mode的一些bug,这正是我们所需要的版本更新。外发的产品不想去更新Firmware,但正在生产的机器想采用FW9.0.1
从Release Note来看,其中的一个更新:
- Support for configurability of Pattern Set Entry index added for Internal Pattern Streaming mode. With this feature the user can choose the starting index of pattern display within a pattern set (index starting from 1)
- 这个更新应该是同步更新了Internal Pattern生成的Flash内容(应该是增加了PatSetEntryIndex内容,也得到的验证)
- 由于API还没有随着FW更新,我们的Internal Pattern内容通过API的接口生成,然后通过I2C写入到Flash。
- Release Notes中,没有相关内容的描述,不知道可否告知,写入到Flash的内容有哪些变更,方便这边正确的修改API
- 我们自己的应用层,想通过版本号来兼容8.0.1与9.0.1
- 类似的帖子:
- DLPC3478: Pattern file generation without GUI, compatible with DLPC firmware 9.0.1 - DLP products forum - DLP®︎ products - TI E2E support forums