This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2000EVM: 無法使用Mplayer播放示例視頻,始終只能投影默認DLPDLCR2000EVM啓動畫面

Part Number: DLPDLCR2000EVM

按照教程(community.element14.com/.../dlp_pico_display_pro_3)使用無桌面環境的BeagleBone Black(寫入的~/image/bone-debian-9.3-lxql-armhf-2018-01-28-4gb.img.xz鏡像)遠程SSH登陸了終端並完成了聯網下載Mplayer等步驟。DLPDLCR2000ECM已經對準插在BBB上并投影默認畫面。能檢測到該設備的地址0x1b和對應寄存器如下。

debian@beaglebone:/opt/scripts/device/bone/capes/DLPDLCR2000$ i2cdetect -y -r 2
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- 1b -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- UU UU UU UU -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

debian@beaglebone:/opt/scripts/device/bone/capes/DLPDLCR2000$ i2cdump -y 2 0x1b
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
10: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
20: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
30: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
90: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
a0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
b0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

但是一直感覺DLPC2607驅動已經初始化存在問題。在完成上面事情以後輸入了一下命令:

i2cset -y 2 0x1b 0x0b 0x00 0x00 0x00 0x00 i

i2cset -y 2 0x1b 0x0c 0x00 0x00 0x00 0x1b i

結果投影畫面還是沒有變化。同時使用i2cget查看對應寄存器值發現還是0x00,貌似根本無法寫入更改0x1b地址對應寄存器的值,手動命令無效。

之後按照教程播放視頻出錯:

debian@beaglebone:/opt/scripts/device/bone/capes/DLPDLCR2000$ python MplayerTest.py
set slave address: 27
Make sure the display port is set. For example export DISPLAY=:0

1
SourceSel.EXTERNAL_VIDEO_PARALLEL_I_F_
2
Resolution.NHD_LANDSCAPE
##################################################################
play video
nhd_test.mp4
MPlayer 1.3.0 (Debian), built with gcc-8 (C) 2000-2016 MPlayer Team
do_connect: could not connect to socket
connect: No such file or directory
Failed to open LIRC support. You will not be able to use your remote control.

Playing nhd_test.mp4.
libavformat version 58.20.100 (external)
libavformat file format detected.
[mov,mp4,m4a,3gp,3g2,mj2 @ 0xb68b4340]Protocol name not provided, cannot determine if input is local or a network protocol, buffers and access patterns cannot be configured optimally without knowing the protocol
[lavf] stream 0: video (h264), -vid 0
VIDEO:  [H264]  640x360  24bpp  30.000 fps  3600.5 kbps (439.5 kbyte/s)
==========================================================================
Opening video decoder: [ffmpeg] FFmpeg's libavcodec codec family
libavcodec version 58.35.100 (external)
Selected video codec: [ffh264] vfm: ffmpeg (FFmpeg H.264)
==========================================================================
Clip info:
 major_brand: mp42
 minor_version: 1
 compatible_brands: mp42avc1
 creation_time: 2017-07-07T14:32:35.000000Z
Load subtitles in ./
Audio: no sound
Starting playback...
Movie-Aspect is undefined - no prescaling applied.
VO: [x11] 640x360 => 640x360 Planar YV12  [fs]
[swscaler @ 0xb6943400]bicubic scaler, from yuv420p to rgb565le using C
[swscaler @ 0xb6943400]No accelerated colorspace conversion found from yuv420p to rgb565le.
[swscaler @ 0xb6943400]using unscaled yuv420p -> rgb565le special converter
V:  22.9   0/  0 54% 51%  0.0% 0 0

Exiting... (End of file)
None
Does the video play on the screen? (Pass/Fail/Stop) (Pass/Fail/Stop) and comment: Test passed

結合之前的錯誤,估計有包括dlpc2607初始化、無法初始化視頻輸出驅動、I2C找不到pctldev、電源控制設備沒有被正確識別等可能原因,具體怎麽解決呢?

  • 这个教程也不是TI 官方的,前端的控制无法提供帮助。

  • 已收到谢谢。前面的问题已解决。目前有个新问题就是买了新的DLPDLCR2000,然后配置好BBB端,DLP2000插上BBB就能显示桌面和播放相关视频了。但是用完直接断电以后第二次插上BBB就发直接D3指示灯不亮,只有D2灯亮。就像是只能使用第一次的DLP2000似的。即使使用命令打开peoj_on的D3端口高电平也只能显示默认画面了,始终没办法如第一次使用一般插上就显示BB的桌面。难道是我第一次输入修改0x1b 地址的两个寄存器数据后再直接断电使得第二次DLP2000开机没办法初始化了吗?还是说有其他的原因