This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP5530Q1EVM: SPI一主多从

Part Number: DLP5530Q1EVM


各位好:

    目前使用DLP230 control program 控制DLP5530光机。

    现在有这样一个需求:用DLP 230 control program 连接cheetah SPI(1个),cheetah SPI连接DLP5530光机(≥2个)。

    我查了cheetah SPI是支持三个从机的通信。想问一下DLP 230 control program 是否支持一主多从模式。

谢谢。