This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3310: 微镜的显示时序

Part Number: DLP3310
Other Parts Discussed in Thread: DLP4710, DLP7000

你好,有如下问题,烦请回答。
问题1:我们有过DLP7000的开发经验,在7000的手册中提到了,可以根据微镜下面RAM中保存的0或1使微镜处于打开或者关闭状态,并且可以做到像素级的控制,可否使用DLp3310或者Dlp4710做一个应用是:想用一个高速的相机去拍DMD,希望打第一张图片的时候,该图片在DLP上保持不动,直到第二张图片来。我很清楚DLp7000可以这样打1bit的图片,不知道Dlp3310或4710是否可以这样做?
问题2:在4710的DLP控制器DLP3479手册中看到了如下图所示,两个位图之间有dark时间,不知道这个dark可否用编程者手册中提到的冻结时间规避?目的同问题1的描述。

问题3:请问在DLP4710的典型应用中并没有一块额外的FPGA,没有看明白数据源应该从哪里进到系统中?只能使用内部的pattern嘛?这个内部的pattern可以修改嘛?