想请问一下,如果不用lightcrafter 4500,而是用DLPC350控制,是不是自己需要做很多电路设计呢?另外lightcrafter 4500可以用在rice大学做的单像素相机的设计吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LightCrafter4500的主芯片是DLPC350. 因此要做成电路板才可以使用. 选择DMD开发板主要考虑:1.速度. 2分辨率.3. DMD 控制放肆:Global and phased or block reset.当然还有DMD翻转方式:是对角线还是side放肆.
Rice University single pixel imaging system has used Discovery 4100. Light crafter 4500主要使用的是Global.因此速度在4225 frame rate/second(最快).
另外4100不带光学系统;4500带有光学系统(因此如果您要去掉光学系统,要花些时间不能损坏电路板和DMD).