DLP230GP: DLP230GP+DLPC3432+DLPA2000

Part Number: DLP230GP
Other Parts Discussed in Thread: DLPA2000, DLPC3432

你好,

        新做的DLP230GP+DLPC3432+DLPA2000方案的驱动板,我们已经能正常点亮投图。

        但是发现开机后(PROJ_ON)会先自动进入DLPC3432的内部测试模式(LED电流约700mA,显示棋盘格图片),初始化成功(HOST_IRQ)后,才能通过IIC控制LED的电流,然后进入外部视频模式。由于内部测试模式电流过大,对电源要求比较高,而且可能会使LED受损。能否提供默认关LED灯的固件。

      我们驱动板上使用了两路DLPC3432( IIC地址分别为0x36和0x3a),使用的是官方的固件“FWSel_DLPC3432_DLPA2000_pm1_i2c0x3a_v7p4p3.img”和“FWSel_DLPC3432_DLPA2000_pm1_i2c0x36_v7p4p3.img”。

谢谢!