This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: U19-M29W128GL70N6F替换料GUI报不支持

Part Number: DLPC350


您好:

    U19-M29W128GL70N6F因停产了,需要找替换料。

    我一开始用了MT28EW128ABA1LJS-0SIT,micron(镁光),在用JTAG FLASH Programmer下载时擦除异常,可编程,可读,校验在0X00000000就出错了,在GUI是无法连接。Connected圆灯一直是红的。

    查了一下,是由于读缓存的大小不一样。

   

     后来用了MX29GL128FLT2I-70G,旺宏电子,用JTAG FLASH Programmer下载时擦除,可编程,可读,校验正常,在GUI可连接,Connected圆灯是绿的。在下载图片时报不支持厂家ID。如下图所示:

     图1:M29W128GL70N6F的FLASH信息

   

     图2:MX29GL128FLT2I-70G的FLASH信息

   

     图3:MX29GL128FLT2I-70G的GUI报错 

   

     怎么才可以让GUI支持这个厂家?

     TI对这个物料的有没有公布的物料列表,我看了3个月前也有人在论坛上问了, 可否把结果也给我说一下,谢谢。

     

  • 你好:

          我更新了用8228.FlashDeviceParameters.txt里的内容更新了FlashDeviceParameters.txt,里面有支持了MT28EW128ABA1LJS-0SIT,micron(镁光)的项,固件GUI图片下载正常,投图正常,但是报下面的错误,如图下所示。请问这个是否影响正常使用?

         还有我在FlashDeviceParameters.txt模仿格式增加了MX29GL128FLT2I-70G,旺宏电子的支持项,但还是在GUI中报不支持。应该怎么让GUI支持这个FLASH?

         谢谢。