This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3000连接不上!!!急求大神们帮助!!



我目前使用的是0.3inch的DLPC3000,这款DLP在我这边原本用GUI 5.0版本是可以正常连接使用的。

上周将此DLP借给朋友使用一周时,他将DLP中的firmware固件升级后也可用GUI 5.0版本软件使用。

但是这周DLP到我这边后,我却不能使用GUI 5.0版本使用。在win7 系统中尝试连接,报错显示:No connection;在XP系统中  连接,报错显示: connection error = 5。

我百思不得其解,还请大家出出主意,提供帮助,谢谢!