入手DLP4500一周了,现在想能够把自己裁剪成912*1140的图片通过operating mode选择video mode,然后下面的video mode选择image from flash。可以选择0~x,选择曝光存储在Flash里的图片。但是要每次选择,怎样才能让它连续曝光存储在Flash中的图片?另外如果每次都往固件添加图片然后更新固件,这样的效率很低啊,我想可以使用视频流的模式,请问这个怎么设置呢?现在是通过vga转hdmi口,vga口接电脑,hdmi口接DLP4500
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
入手DLP4500一周了,现在想能够把自己裁剪成912*1140的图片通过operating mode选择video mode,然后下面的video mode选择image from flash。可以选择0~x,选择曝光存储在Flash里的图片。但是要每次选择,怎样才能让它连续曝光存储在Flash中的图片?另外如果每次都往固件添加图片然后更新固件,这样的效率很低啊,我想可以使用视频流的模式,请问这个怎么设置呢?现在是通过vga转hdmi口,vga口接电脑,hdmi口接DLP4500
那你进步蛮快的.
请参考: http://www.ti.com/tool/dlplcr4500evm
第25页.
根据29页,可以修改触发和曝光时间来更改刷新率.
• Set Pattern Exposure: 100000 μs
• Set Image Load Time: 200000 μs
http://www.ti.com/tool/dlplcr4500evm