Lightcrafter 4500 能够通过编程实现在线生成投影的图案吗? 已配置Pandaboard 4500。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lightcrafter 4500 能够通过编程实现在线生成投影的图案吗? 已配置Pandaboard 4500。谢谢!
D4100 Kit是一个开发平台., 具有很大的可扩展性和可编程功能, 可以通过软件将图片下载(USB)到FPGA控制的大容量DDR2中.但是这一切要根据你的功能定义来编写程序实现的.
请参考pandaboard4500规格书:(注意和一般pandaboard有些不一样的.专门为lightcrafter4500配合的)
http://www.ti.com/devnet/docs/catalog/endequipmentproductfolder.tsp?actionPerformed=productFolder&productId=16961
你好:
目前我们也是面临和你们同样的问题,只不过我们又购买的6500,同样不知道如何实现,如果你们有啥建议,咱们可以沟通一下
电话:15191891713
邮箱:jiang123fuyi@163.com
4500存储不了大量的图片。要想大量存储图片只能用Discovery 4100.
D4100是一个开放的平台,能实现你所需要的功能。
tel:0396-5970858
e-mail:sales@jinfeitech.com
website:www.jinfeitech.com
不管是4500,还是6500及9000,都是不能存储大量的图片,他们都是采用的投影机的DLP方案,是用来显示彩色或者灰度图像的,如果要显示二进制图像,只能将二进制图像存储在板载Flash中。
4500,还是6500及9000上板载的存储器是Flash,空间很有限,存储不了大量图像。
如果要存储大量的图片,建议用D4100。
tel:0396-5970858
e-mail:sales@jinfeitech.com
website:www.jinfeitech.com